< Assembler Command Options / Microcontroller Options >
When -patch=rx610 is specified, the MVTIPL instruction which causes a problem in the RX610 Group is handled as an undefined instruction. The MVTIPL instruction will not be recognized as an instruction and the error message E0552113 will be output. |