< Optimizing Linkage Editor (rlink) Options / Input Options >
The numerical value is specified in the hexadecimal notation. If the specified value starts with a letter from A to F, symbols are searched first, and if no corresponding symbol is found, the value is interpreted as a numerical value. Values starting with 0 are always interpreted as numerical values. |
If the specified symbol name is a C/C++ variable name, add an underscore (_) at the head of the definition name in the program. If the symbol name is a C++ function name (except for the main function), enclose the definition name with the double-quotes including parameter strings. If the parameter is void, specify as "<function name>( )". |
define=_sym1=data ; Defines _sym1 as the same value as the externally defined symbol data. define=_sym2=4000 ; Defines _sym2 as 0x4000. |