< Optimizing Linkage Editor (rlink) Options / Output Options >
When this option is omitted, debugging information is output to the output file.
If debug is specified and if two or more files are specified to be output with output, they are interpreted as sdebug and debugging information is output to <first output file name>.dbg. |
When form={object | library | hexadecimal | stype | binary}, strip or extract is specified, this option is unavailable. |