< Optimizing Linkage Editor (rlink) Options / Other Options >
For a C/C++ variable name or C function name, add an underscore (_) at the head of the definition name in the program. For a C++ function name, enclose the definition name in the program with double-quotes including the parameter strings. If the parameter is void, specify as "<function name>()". If there are several files or modules of the same name, the file that is input first is applied. |
When a symbol is deleted using this option, the object is not deleted but the attribute is changed to the internal symbol. |
delete=(_sym1) ; Deletes the symbol _sym1 in all files. delete=file1.obj(_sym2) ; Deletes the symbol _sym2 in the file file1.obj. |
When form={absolute|relocate|hexadecimal|stype|binary} has been specified, this option deletes external symbols. |
Operation is not guaranteed if this option is used in combination with compile option -merge_files. |