< Optimizing Linkage Editor (rlink) Options / Options Other Than Above >
Executes option strings specified before END. After the linkage processing is terminated, option strings that are specified after END are input and the linkage processing is continued. |
input=a.obj,b.obj ; Processing (1) start=P,C,D/100,B/8000 ; Processing (2) output=a.abs ; Processing (3) end input=a.abs ; Processing (4) form=stype ; Processing (5) output=a.mot ; Processing (6) |
Executes the processing from (1) to (3) and outputs a.abs. Then executes the processing from (4) to (6) and outputs a.mot. |