< Library Generator Options / Library Options >
When reentrant libraries are linked, use #define to define the macro name of _REENTRANT before including standard include files in the program or use the -define option to define _REENTRANT at compilation. |