The position within a new file should be calculated and set using the following methods, depending on the third parameter (base). |
(1) When base is 0: Set the position at offset bytes from the file beginning
(2) When base is 1: Set the position at the current position plus offset bytes
(3) When base is 2: Set the position at the file size plus offset bytes
When the file is a console, printer, or other interactive device, when the new offset is negative, or when in cases (1) and (2) the file size is exceeded, an error occurs. |
When the file position is set correctly, the new position for reading/writing should be returned as an offset from the file beginning; when the operation is not successful, -1 should be returned. |
Normal: The new position for file reading/writing, as an offset in bytes
from the file beginning
offset Position for reading/writing, as an offset (in bytes)
base Starting-point of the offset