1.1 Overview

When debugging programs using the RI600V4 functionality, it is possible to use the resource information tool to confirm the RI600V4 resource information (e.g. system information and memory area information) that changes dynamically as the program executes.