A.1 Description

Windows/panels/dialog boxes for debugging are listed below.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Description

Main window

Controls the program execution. Various windows, panels and dialog boxes can be opened from this window.

Debug Manager panel

Selects a core (PE) to be debugged and displays the core status.

Project Tree panel

Selects the debug tool to use.

Property panel

Displays detailed information on the debug tool currently selected in the Project Tree panel, and enables the settings of the tool to be changed.

Memory panel

Displays and modifies memory values.

Disassemble panel

Displays the results of memory value disassemble and is used to execute line assemble and instruction level debug.

CPU Register panel

Displays the contents of CPU registers, and modifies register values.

IOR panel

Displays and modifies I/O register values.

Local Variables panel

Displays and modifies local variables.

Watch panel

Displays and modifies registered watch-expression values.

Call Stack panel

Displays call stack information on function calls.

Trace panel

Displays trace data acquired from the debug tool.

Events panel

Displays detailed information on set events, switches the events between enabled and disabled, or deletes them.

Output panel

Displays messages output from the build tool/debug tool/plug-ins, or the results of batch searches carried out using the Find and Replace dialog box.

Select I/O Modules dialog box

Sets the I/O modules which details are displayed.

Memory Mapping dialog box

Displays the memory mapping.

Download Files dialog box

Selects files to be downloaded and sets the download conditions.

Flash Options Setting dialog box

Configures options for the flash memory.

Action Events dialog box

Sets action events.

Column Number Settings dialog box

Specifies the number of view columns of memory values on the Memory panel.

Address Offset Settings dialog box

Specifies an offset value for the address display on the Memory panel.

Memory Initialize dialog box

Initializes memory.

Memory Search dialog box

Searches memory.

Print Address Range Settings dialog box

Sets the address range to print the contents of the Disassemble panel.

Trace Search dialog box

Searches trace data.

Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20]

Displays and modifies the detailed information on the point trace event.

Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20]

Displays and modifies the detailed information on the timer event.

Detailed Settings of Performance Measurement dialog box [Full-spec emulator][E1][E20]

Displays and modifies the detailed information on the Performance Measurement event.

Scroll Range Settings dialog box

Sets the scroll range for the Memory panel/Disassemble panel.

Go to the Location dialog box

Moves the caret to the specified position.

Data Save dialog box

Saves the settings and other data displayed in the respective windows/panels/dialog boxes or saves upload data.

Specified Section dialog box

Specifies the range for skipping step execution.

Functions and Variables Access Table panel

Displays the functions that access variables in the form of an orthogonal table.

Exclusive Control Checking Tool dialog box

Checks whether exclusive control is correctly performed for a certain variable and makes the settings required for checking.

Pseudo-Error Debugging panel [Full-spec emulator][E1][E20]

This panel is central to the functionality of the solution for pseudo-error debugging.

Select Pseudo-Error dialog box [Full-spec emulator][E1][E20]

Selects ECM pseudo-errors displayed in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20].

Breakpoint Setting dialog box [Full-spec emulator][E1][E20]

Sets the breakpoints that are to be registered to the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20].

Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20]

This panel is central to the functionality of the solution for debugging of CAN bus reception.

RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20]

Makes settings related to the entire RS-CAN module.

Receive Channel Setting dialog box [Full-spec emulator][E1][E20]

Makes settings related to the receive channel.

Transmit Channel Setting dialog box [Full-spec emulator][E1][E20]

Makes settings related to the transmit channel.

Transmit Frame Setting dialog box [Full-spec emulator][E1][E20]

Makes settings related to the transmit frame.

Measuring CAN Bus Reception Processing Times panel [E2]

This panel is central to the functionality of the solution for measurement of CAN bus reception processing times.

Measurement Condition Setting dialog box [E2]

This dialog box is used to set conditions for measurement in the Measuring CAN Bus Reception Processing Times panel [E2].