2.13.4.3 Edit a Point Trace event [Full-spec emulator][E1][E20]

Detailed information on a Point Trace event is edited in the Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20]. This dialog box is opened by selecting the Point Trace event you desire to edit on the Events panel then selecting [Edit Condition...] from the context menu.

(1)

When editing an address condition

The start address and end address can be specified as an address condition in the Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20].

(2)

When editing an event target

The following can be specified as an event target in the Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20].

Event Target

Function

CPU

Access to the CPU is the target of the point trace.

Global RAM

Access to the Global RAM is the target of the point trace.

Cluster RAM

Access to the Cluster RAM is the target of the point trace.