Detailed information on a Point Trace event is edited in the Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20]. This dialog box is opened by selecting the Point Trace event you desire to edit on the Events panel then selecting [Edit Condition...] from the context menu.
The start address and end address can be specified as an address condition in the Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20].
The following can be specified as an event target in the Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20].