2.18.6.2  
Event types that can be set and deleted during execution
 
The following types of events can be set or deleted during program execution, or during tracer/timer execution.
| 
Table 2.22 | Event Types That Can be Set and Deleted during Execution  | 
|  |  | 
|  |  |  | 
| 
Hardware Break (execution type: after execution)
 |  |  | 
| 
Hardware Break (execution type: before execution)
 |  |  | 
| 
Hardware Break (access type)
 |  |  | 
| 
Software Break |  |  | 
| 
Trace (trace start/trace end)
 |  |  | 
| 
Point Trace |  |  | 
| 
Timer Result(timer start/timer end)
 |  |  | 
| 
Performance Measurement (performance measurement start/
 performance measurement end)
 |  |  | 
| 
Action (Printf)
 |  |  | 
 
 : Possible, if the program execution is allowed to pause for eventsNote
 		: Possible, if the program execution is allowed to pause for eventsNote
 : Impossible while tracer or timer is executing
 		: Impossible while tracer or timer is executing 
NG 		: Impossible
 : Not supported
 		: Not supported
| 
Note | To enable this, specify [Yes] with the [Set event by stopping execution momentarily] property in the [Set Event While Running] category on the [Debug Tool Settings] tab of the Property panel.  |