2.20.3  Icons for invalid input 
 
In some of the dialog boxes in CS+, the 
 icon will appear at a point where incorrect characters are entered as a warning sign.
Remark  | Placing the cursor over the  
 icon will pop up the information that indicates the characters to be entered.  |