The cause of the break other than the described above is as follows:
You can confirm the break cause with the Status message on the statusbar in the Main window, Output panel, or Trace panel [Simulator].
The operation depends on the setting of the [Operation after trace memory is full] property in the [Trace] category on the [Debug Tool Settings] tab of the Property panel.  | 
A break for a synchronous execution and a synchronous break, in a microcontroller that supports multi-core  |