2.6.2.2 Change display format

The display format of the disassemble area can be changed using buttons below on the toolbar.

View

The following buttons to change the display format are displayed.

 

Show Offset

Displays the offset value of the label. The offset value from the nearest label is displayed when a label is defined for the address.

Show Symbol

Displays the address value as the result of disassembling in the format "symbol + offset value" (default).

Note that when a symbol has been defined as the address value, only the symbol is displayed.

Show Function Name

Displays the name of the register by its function name (default).

Show Absolute Name

Displays the name of the register by its absolute name.