2.7 Execute Programs

This section describes how to execute programs.

Main operations in this section are taken place from the debug toolbar or the [Debug] menu in the Main window, where commands to control the execution of programs are included.

Caution

Items of the debug toolbar and the [Debug] menu are valid only while connected to the debug tool.

Figure 2.78

Debug Toolbar

Figure 2.79

[Debug] Menu