To configure serial communication, click the
on the Simulator GUI window's toolbar. The following Serial window opens.
This window provides serial I/O features for communicating with the CPU's built-in serial interface. This enables you to input data to the microcontroller's serial receiver pin, and acquire output data from its serial transmitter pin.
See the section on the Serial window for details about controlling the window.