B. I/O FUNCTIONS

This section describes the I/O settings for the simulator in a low-level interface routine (assembly language part).

The simulator provides functions for handling standard I/O and file I/O

The I/O function for a simulator can be used when [Simulator mode] is specified in the [Select stream I/O mode] property in the [Stream I/O] [Simulator] category on the Property panel's [Debug Tool Settings] tab.