2.17.2 Displaying only a specific type of event

By clicking one of the following toolbar buttons, it is possible to display only a specific type of event.

 

Displays hardware break-related events.

 

[E1] [E20] [EZ Emulator]

Displays software break-related events.

 

Displays trace-related events.

 

Displays timer-related events.

 

Displays action events (Printf event, interrupt event [Simulator]).

 

Displays built-in events (unconditional trace event or Run-Break timer event). Note

Note

The EZ Emulator does not support Run-Break timer events.