2.14.2.2
Checking the Events panel for confirmation
When a program has stopped running, the measurement result is displayed as a Run-Break timer event on the Events panel that is opened by selecting [Event] from the [View] menu.
Figure 2.155 | Example of a Run-Break Timer Event Measurement Result (Events Panel) [E1] [E20] |
Figure 2.156 | Example of a Run-Break Timer Event Measurement Result (Events Panel) [Simulator] |