2.10.6
Other break factors
Other than the causes described above, a program can be stopped by the following break factors.
You can check such break factors on the Status bar in the Main window.
Table 2.7 | Other break factors |
|
|
|
|
|
Trace memory fullNote 1
|
|
|
|
Temporary break occurred
|
|
|
|
Execution failed or cause unknown
|
|
|
|
WAIT Instruction executed
|
|
|
|
Undefined instruction exception encountered
|
|
|
|
Privileged instruction exception encountered
|
|
|
|
Access exception encountered
|
|
|
|
Floating-point exception encountered
|
|
|
|
Interrupt encountered
|
|
|
|
INT instruction exception encountered
|
|
|
|
BRK instruction exception encountered
|
|
|
|
Peripheral function simulation error occurred
|
|
|
|
Illegal memory access made
|
|
|
|
Stream I/O error occurred
|
|
|
|
Allocation of coverage memory failed
|
|
|
|
Allocation of trace memory failed
|
|
|
|
E2 expansion function
|
|
|
|
Fully used the storage memory
|
|
|
|
Note 3. | [Simulator]
A single-precision floating-point exception can be the object of this factor.
|