2.4.1 Highlight the current line

By selecting the [Enable line highlight for current] check box in the []General - Text Editor] category of the Option dialog box, the current line (i.e. line at the current caret position) can be displayed within a rectangle (the rectangle color depends on the highlight color in the [General - Font and Color] category of the Option dialog box).

Figure 2.5

Highlighting Current Line

Remark

The rectangle color depends on the highlight color in the [General - Font and Color] category of the Option dialog box.