A.1 Overview

The Pin Configurator has the following windows, panels and dialog boxes.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Function

Main window

This is the first window to open when CS+ is launched. This window is used to operate various components (design tool, build tool, etc.) provided by CS+.

Project Tree panel

This panel displays the components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

Property panel

This panel allows you to view the information on and change the setting for the node selected in the Project Tree panel.

Device Pin List panel

This panel allows you to enter information on each pin of the microcontroller.

Device Top View panel

This panel displays the information entered in the Device Pin List panel.

Output panel

This panel displays operation logs for various components (design tool, build tool, etc.) provided by CS+.

Column Chooser dialog box

This dialog box allows you to choose whether or not to display the item listed in this dialog box in the device pin list, and add columns to or delete columns from the device pin list.

New Column dialog box

This dialog box allows you to add your own column to the device pin list.

Save As dialog box

This dialog box allows you to name and save a file.