This tab displays information (Product Information) on the [Pin View)] selected in the Project Tree panel.
The following items are explained here.
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View], and then select [Property] from the [View] menu. |
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View], and then select [Property] from the context menu. |
If this panel is already open, selecting a different [Pin View] in the Project Tree panel changes the content displayed accordingly. |
This area displays product information (Version and Release date) on Code Generator.
Displays the release date of Code Generator (Code Generator 2 Plug-in). |
|
Displays the version of Code Generator (Code Generator 2 Plug-in). |