|
build.Link.AdditionalOptions
|
This property sets or refers to the link options for the active project regarding other additional options.
[Specification format]
build.Link.AdditionalOptions = option
|
[Setting(s)]
|
|
|
|
option
|
Set the additional link options as strings.
|
[Reference]
Additional link options (strings)
[Detailed description]
- | This property sets or refers to the link options for the active project regarding other additional options. |
- | The options set here are added at the end of the link options group. |
[Example of use]
>>>build.Link.AdditionalOptions = "-stack -Total_size" ... Set multiple options
>>>print build.Link.AdditionalOptions
-stack -Total_size
>>>lopt = build.Link.AdditionalOptions + " -map=file.bls" ... Refer the current setting and add an option
>>>build.Link.AdditionalOptions = lopt
>>>print build.Link.AdditionalOptions
-stack -Total_size -map=file.bls
>>>
|