1. GENERAL

CS+ is an integrated development environment for use with microcontrollers. The Python console can control CS+ using IronPython (Python that runs on .NET Framework) which is a script language. The functions, properties, classes, and events to control CS+ are added to the Python console.

 

This manual describes the usage of the Python console and the functions, properties, classes, and events that have been extended for CS+.

 

===========

This software includes the work that is distributed in the Apache License 2.0.

http://www.apache.org/licenses/LICENSE-2.0

===========

Caution

The above Web site may not be displayed from this document.