A.1 Description

Below is a list of the panel related to the Python console.

Table A.1

Panel List

Panel Name

Function Description

Python Console panel

You can use IronPython to operate CS+ and the debug tool by command input. You can also register a script with the project by simply displaying the sample script.