Rebuild the program of loaded sample project.
1. Build project
In this step, rebuild the program of loaded sample project.
Click the [Rebuild Project.] button. |
Check to see if the rebuild process has been completed correctly. If the build process has been completed correctly, a load module file is created. |