This section describes an overview of the program you will create in this tutorial and the target board (QB-R5F100LE-TB).
1. Overview of the Program
You are going to create a simple program which causes two LEDs flash alternately. See "Description of Sample Program" for details on this program.
Two LEDs flash alternately
2. Overview of the target board (QB-R5F100LE-TB)
The following is an overview of QB-R5F100LE-TB which will be used as a target board. See "Specifications of QB-R5F100LE-TB" in Appendix for details on QB-R5F100LE-TB.
Evaluation LED1 : Lights in yellow when the port 62 (P62) is LOW.
Evaluation LED2 : Lights in yellow when the port 63 (P63) is LOW.
14pin connector : Used for on-chip debugging and programming.