In this section, you edit the user program.
First, the basic editing method is explained, and then you edit the program through a simple copy and paste procedure. Edit the program following the steps listed below.
1. How to open a source code file
The following step describes how to open a source code file.
Find the source code file you want to edit in the Project Tree and double-click it. |
This displays the source code in the Main panel. |