Procedure to Create a Program

This section describes a procedure to create a program.

Start performing the task after installing CS+.

(1) Generate code

:Configure the peripheral functions built in the microcontroller you are going to use. After completing configuration, generate the code.

(2) Coding

:Edit the program

(Copy and paste the sample program).

(3) Build

:Build the program

(If an error occurs, edit the program again).

(4) Debugging

:Debug the program using R0K505111S000BE

and E1.

(5) Writing

: Write a program to the microcontroller using E1