This section describes a procedure to create a program.
Start performing the task after installing CS+.
|
(1) Open the sample program :This time, you dont use the code-generation functions. Instead, you must read out a program from a sample program. |

|
(2) Coding :Since you use a sample program, you dont edit the program. Here, we describe how to perform basic operations. |

|
(3) Build :Build the program (If an error occurs, edit the program again). |

|
(4) Debugging :Debug the program using R0K556100S000BE and E1. |

|
(5) Writing : Write a program to the microcontroller using E1 |