2. Create a category
This section describes how to create a category.
Users can categorize files freely.
From the project tree, right click a file, then select [Add] → [Add New Category]. |
[New Category] is created as shown in the figure below. You can change the name to anything you like. As an example, here we name the category [Source File]. |
Drag [hwsetup.c], and drop it onto [Source Files]. [hwsetup.c] is now categorized as [Source Files]. |
We created two categories as an example. |