This section describes an overview of the program you will create in this tutorial and Renesas Starter Kit for RX65N-2MB (RTK50565N2S10000BE ).
1. Overview of the Program
You are going to create a simple program which causes two LEDs flash alternately. See "Description of Sample Program" for details on this program.
Two LEDs flash alternately
2. Overview of Renesas Starter Kit for RX65N-2MB (RTK50565N2S10000BE )
The following is an overview of RTK50565N2S10000BE which will be used as a target board.
Please set up the switches as follows.
See "Specifications of RTK50565N2S10000BE" in Appendix for details on RTK50565N2S10000BE.
Evaluation LED0 : Lights in yellow when the port 73 (P73) is LOW.
Evaluation LED1 : Lights in yellow when the port G7 (PG7) is LOW.
E1/E2 Lite(14pin connector) : Used for on-chip debugging.
Switch
SW4 Pin1 :OFF (Single chip mode)