This page displays a list of selected updates, and starts the download process.
The following items are explained here.
From the CS+ Update Manager window menu area, click [Download only]. |
From the Select updates page main area, click [Download only]. |
This button is disabled if no updates are selected.
Displays a list of items to update.
The following information is displayed for each update.
This appears if there is detailed information about the update. Selecting it will display details in a browser. |