This dialog box is used to add existing files and folder hierarchies to the project.
The folder is added as a category.
The following items are explained here.
Drag the folder from Explorer or the like, and drop it on the Project Tree panel. |
Select the type of the file to be added to the project.
You can select multiple file types by left clicking while holding down the [Ctrl] or [Shift] key.
If nothing is selected, it is assumed that all types are selected.
Directly enter the number of levels of the subfolder to be added to the project.
Up to 10 (decimal number) can be specified. |
Adds the folder that was dragged and dropped and the files in that folder to the project. And then closes this dialog box. |
|
Does not add the folder and files, and then closes this dialog box. |
|