Other Windows... dialog box


This dialog box is used to select one of the divide panels shown in the Main window to activate or close.

Figure A.64

Other Windows... Dialog Box

 

The following items are explained here.

[How to open]

-

From the [Window] menu, select [Other Windows...].

Remark

[Other Windows...] only appears when ten or more divide panels are open.

[Description of each area]

(1)

Select divide panel area

Selecting a divide panel switches the target.

[Function buttons]

Button

Function

Activate

Activates the divide panel selected in the Select divide panel area, and close this dialog box.

Close Window(s)

Closes the divide panel selected in the Select divide panel area, and close this dialog box.

Close

Closes this dialog box.