2.4.5 Change the project name

You can change the name of the project (main project or subproject) on the project tree.

Select the Project node or Subproject node and select [Rename] on the context menu.

Figure 2.22

[Rename] Item (For a Project)

 

Remark

After changing the project name, when you save the project, the actual name of the project file is also changed.