3.4 Information

Table 3.4

Information

M0190000

[Message]

Failed to read license information. The file is broken.

Please re-enter license keys.

M0190010

[Message]

The version of the license manager you are using is older than that assumed by the floating license server.

Update the license manager.

M0190011

[Message]

The version of the floating license server you are using is older than that assumed by the license manager.

Update the floating license server.

M0191000

[Message]

Critical Error : XXX

M0191100

[Message]

Critical Error : XXX

M0191200

[Message]

Error : XXX

M0191300

[Message]

Error : XXX

M0191400

[Message]

Warning : XXX

M0191500

[Message]

Warning : XXX

M0191600

[Message]

Required license : XXX

M0191601

[Message]

Local license found.

M0191602

[Message]

Needs renewal.

M0191603

[Message]

Expired.

M0191604

[Message]

Invalid.

M0191605

[Message]

Released.

M0191606

[Message]

Upper level licesne : XXX

M0191607

[Message]

Get new licesne : XXX

M0191608

[Message]

Supported : XXX licenses

M0191700

[Message]

Request : XXX

M0191701

[Message]

Add client : XXX

M0191702

[Message]

Delete client : XXX

M0191703

[Message]

Client unknown.

M0191704

[Message]

Server id is invalid.

M0191705

[Message]

Target license is empty.

M0191706

[Message]

Upper level license is available

M0191707

[Message]

Assigned license (XXX/XXX) : XXX

M0191708

[Message]

Expired license : (XXX/XXX) : XXX

M0191709

[Message]

Released license : (XXX/XXX) : XXX

M0191800

[Message]

Command : XXX

M0191801

[Message]

Getting license : XXX

M0191802

[Message]

Connecting : XXX

M0191803

[Message]

Getting upper level license : XXX

M0191804

[Message]

Getting supported licenses : XXX

M0191805

[Message]

Getting license as offline mode : XXX

M0191806

[Message]

Releasing license : XXX

M0191900

[Message]

Starting service.

M0191901

[Message]

Starting HTTP listener.

M0191902

[Message]

Received HTTP request.

M0191903

[Message]

Received next request.

M0191904

[Message]

Getting license list.

M0191950

[Message]

Stop service.

M0191951

[Message]

Stop HTTP listener.

M0191952

[Message]

Bad HTTP request.

M0191953

[Message]

Unknown request.

M0191954

[Message]

Unkown client.

M0191955

[Message]

Invalid server ID.

M0191956

[Message]

Invalid : XXX

M0191957

[Message]

Released : XXX