This tab shows the detailed information on each C source file, assembly source file, object file, and library file categorized by the following and the configuration can be changed.
[Description of each category]
The detailed information on the build is displayed and the configuration can be changed.
|
Select whether to set the compile option that differs from the project settings to the selected C source file. If [Yes(Level 3)(Perform with assuming it the whole program)(-Xwhole_program)] is selected in the [Perform inter-module optimization] property in the [Optimization(Details)] category from the [Compile Options] tab, this property will be grayed out and changed to [No]. This property is displayed only when a C source file is selected on the project tree and [Yes] in the [Set as build-target] property from this tab is selected. |
||||
|
Sets the option that differs from the project settings to the selected C source file. |
||||
|
Does not set the option that differs from the project settings to the selected C source file. |
||||
|
Select whether to set the assemble option that differs from the project settings to the selected assembly source file. If [Yes(Level 3)(Perform with assuming it the whole program)(-Xwhole_program)] is selected in the [Perform inter-module optimization] property in the [Optimization(Details)] category from the [Compile Options] tab, this property will be grayed out and changed to [No]. This property is displayed only when the assembly source file is selected on the project tree and [Yes] in the [Set as build-target] property from this tab is selected. |
||||
|
Sets the option that differs from the project settings to the selected assembly source file. |
||||
|
Does not set the option that differs from the project settings to the selected assembly source file. |
||||
|
C source file (when the C source file is selected) Assembly source file (when the assembly source file is selected) |
||||