This tab shows the detailed information on the build tool categorized by the following and the configuration can be changed.
(1) [Build Mode]
(2) [Build]
(3) [Build Method]
(4) [Path of Tools]
(5) [Notes]
Remark | For details on compiler driver options, refer to "MULTI: Building Applications for Embedded V850 and RH850" released by Green Hills Software, LLC. Please do not contact Green Hills Software, LLC with any inquiries about the CCRH850 build-tool plugin of CS+. |
Caution 1. | This tab is displayed only when the current project has been created with [Using Existing GHS Project File(GHS CCRH850)] selected as the project type. |
Caution 2. | If you have upgraded the GHS compiler version, confirm the setting of the [Compiler package folder] property from the [Path of Tools] category. |
[Description of each category]
The detailed information on the build mode is displayed and the configuration can be changed.
Build mode
|
Select the build mode to be used during a build.
Note that this property is not applied to [Reset All to Default] from the context menu.
|
Default
|
DefaultBuild
|
How to change
|
Select from the drop-down list.
|
Restriction
|
DefaultBuild
|
Runs a build with the default build mode that is set when a new project is created.
|
Build mode that is added to the project
|
Runs a build with the build mode that is added to the project (other than DefaultBuild).
|
Change property value for all build modes at once
|
Select whether to reflect the value newly set to all build modes when a value is set in this property.
Be careful since the value set may not be an appropriate value for other build modes.
|
Default
|
No
|
How to change
|
Select from the drop-down list.
|
Restriction
|
Yes
|
Reflects the value newly set to all build modes when a value is set in this property.
|
No
|
Does not reflect the value newly set to all build modes when a value is set in this property.
|
The detailed information on the build is displayed and the configuration can be changed.
MULTI project file to be built
|
Specify the MULTI project file referred when building a project.
This is common to all the build modes.
The following placeholders are supported.
%ActiveProjectDir%: Replaces with the absolute path of the active project folder.
%ActiveProjectName%: Replaces with the active project name.
%BuildModeName%: Replaces with the build mode name.
%MainProjectDir%: Replaces with the absolute path of the main project folder.
%MainProjectName%: Replaces with the main project name.
%MicomToolPath%: Replaces with the absolute path of the install folder of this product.
%ProjectDir%: Replaces with the absolute path of the project folder.
%ProjectName%: Replaces with the project name.
%TempDir%: Replaces with the absolute path of the temporary folder.
%WinDir%: Replaces with the absolute path of the Windows system folder.
|
Default
|
Blank
|
How to change
|
Directly enter in the text box or edit by the Specify MULTI Project File dialog box which appears when clicking the [...] button.
|
Restriction
|
Up to 259 characters
|
MULTI top project file to be built
|
Specify the MULTI top project file referred when building a project.
This is common to all the build modes.
The following placeholders are supported.
%ActiveProjectDir%: Replaces with the absolute path of the active project folder.
%ActiveProjectName%: Replaces with the active project name.
%BuildModeName%: Replaces with the build mode name.
%MainProjectDir%: Replaces with the absolute path of the main project folder.
%MainProjectName%: Replaces with the main project name.
%MicomToolPath%: Replaces with the absolute path of the install folder of this product.
%ProjectDir%: Replaces with the absolute path of the project folder.
%ProjectName%: Replaces with the project name.
%TempDir%: Replaces with the absolute path of the temporary folder.
%WinDir%: Replaces with the absolute path of the Windows system folder.
|
Default
|
Blank
|
How to change
|
Directly enter in the text box or edit by the Specify MULTI Project File dialog box which appears when clicking the [...] button.
|
Restriction
|
Up to 259 characters
|
Additional option on cleaning
|
Specify the additional option to the command line when cleaning a project.
This is common to all the build modes.
|
Default
|
-clean
|
How to change
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button.
|
Restriction
|
Up to 259 characters
|
The detailed information on the build method is displayed and the configuration can be changed.
Build in parallel
|
Select whether to enable the parallel build facility.
The parallel build facility enables CS+ to compile/assemble multiple source files in parallel using all processors mounted on the computer. This speeds up compilation/assemble.
In addition, parallel build between projects can be set by selecting [Tool] menu >> [Option] and then making a setting in the [General - Build] category of the Option dialog box.
This corresponds to the -parallel option of the gbuild command.
|
Default
|
No
|
How to change
|
Select from the drop-down list.
|
Restriction
|
Yes
|
Enables the parallel build facility.
|
No
|
Disables the parallel build facility.
|
The detailed information on the path of tools is displayed and the configuration can be changed.
Compiler package folder
|
Specify the folder of the compiler package to be used.
This is common to all the build modes.
|
Default
|
Value-according-to-installation-environment
|
How to change
|
Directly enter in the text box or edit by the Browse For Folder dialog box which appears when clicking the [...] button.
|
Restriction
|
Up to 247 characters
|
Executable file name for building
|
Specify the executable file name for building.
This is common to all the build modes.
|
Default
|
gbuild.exe
|
How to change
|
Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button.
|
Restriction
|
Up to 259 characters
|
The detailed information on notes is displayed and the configuration can be changed.
Memo
|
Add memos to the build tool.
Add one item in one line.
This setting is common to all the build modes.
The specified memo is displayed as the subproperty.
|
Default
|
Memo[number-of-items]
|
How to change
|
Edit by the Text Edit dialog box which appears when clicking the [...] button.
For the subproperty, you can enter directly in the text box.
|
Restriction
|
Up to 256 characters
Up to 256 items can be specified.
|