The macros supported in the CA78K0R are converted as follows. If there is no corresponding macro in the CC-RL, the CcnvCA78K0R outputs a message. The CPU macro is not converted and no message is output.
Table 3.1 | Conversion of Macro Names |
|
|
|
|
|
__LINE__
|
Not converted
|
Can be used in the CC-RL without any change.
|
|
__FILE__
|
Not converted
|
Can be used in the CC-RL without any change.
|
|
__DATE__
|
Not converted
|
Can be used in the CC-RL without any change.
|
|
__TIME__
|
Not converted
|
Can be used in the CC-RL without any change.
|
|
__STDC__
|
Not converted
|
Can be used in the CC-RL without any change.
|
|
__K0R__
|
__RL78__
|
|
|
__K0R_SMALL__
|
__RL78_SMALL__
|
|
|
__K0R_MEDIUM__
|
__RL78_MEDIUM__
|
|
|
__K0R_LARGE__
|
Not converted
|
A message is output.
Handled as a user-defined macro in the CC-RL.
|
|
__CHAR__UNSIGNED__
|
__UCHAR
|
|
|
__RL78__
|
Not converted
|
Can be used in the CC-RL without any change.
|
|
__RL78_1__
|
__RL78_S2__
|
|
|
__RL78_2__
|
__RL78_S3__
|
|
|
__RL78_3__
|
__RL78_S1__
|
|
|
__CA78K0R__
|
Not converted
|
A message is output.
When the -convert_cc option is used in the CC-RL, define the __CA78K0R__ macro.
|
|
CPU macro
|
Not converted
|
A message is not output.
Handled as a user-defined macro in the CC-RL.
|