When the message number type is information, the information types are classified as follows.
Table 4.2 | Information Types |
|
|
|
|
Change
|
Changes were made in the program so that it can be handled by the CC-RL.
|
|
Insert
|
Additions were made in the program so that it can be handled by the CC-RL.
|
|
Delete
|
Some descriptions were deleted because they are not necessary in the CC-RL.
|
|
Info
|
Conversion may not be sufficient in some cases because of the difference between the CA78K0R and CC-RL specifications.
Each case should be confirmed individually.
|