|
|
|
|
|
E0591001
|
Multiple input files are not allowed.
|
Only one input file can be specified.
Use the list file to specify multiple input files.
|
|
E0591002
|
The option option cannot have an argument.
|
An argument was specified for an option that should not have arguments.
|
|
E0591003
|
The option option requires an argument.
|
No argument was specified in an option that requires arguments.
|
|
E0591004
|
The option option is specified more than once.
|
Only one option can be specified at one time.
|
|
E0591005
|
Requires an output file.
|
The output file corresponding to the input file was not specified.
|
|
E0591006
|
Failed to read an input file file.
|
The folder name or file name may be incorrect. If the next file is specified in the list file, conversion of that file will start.
|
|
E0591007
|
Failed to write a result of conversion file file.
|
The folder name may be incorrect.
|
|
E0591008
|
Failed to write an output file file.
|
The folder name may be incorrect.
|
|
E0591009
|
Failed to read a list file file.
|
The folder name may be incorrect.
|
|
E0591010
|
Syntax errors in list file file.
|
The description of the list file is not correct.
|
|
E0591011
|
File name is corrupted.
|
There are duplicate file names among the input file, output file, and conversion result output file.
|
|
E0591012
|
Invalid file name.
|
Either the input file name specified on the command line or an input or output file name specified in the list file has exceeded 260 characters.
|
|
E0591013
|
Invalid argument for the option option.
|
The argument specification is invalid or the specified file name has exceeded 260 characters.
|
|
E0591101
|
Illegal syntax in string.
|
Conversion could not be performed because there was a syntax that is not allowed in the CA78K0R. Modify the input file.
|
|
E0591102
|
Can not add inline function for assembly.
|
The number of inline functions for assembly has exceeded the upper limit. Modify the input file.
|
|
E0591103
|
Failed to delete a temporary file.
|
Deletion of a temporary file has failed. Delete the temporary file.
|