Reads the results of A/D conversion (16 bits; most significant 16 bits of 24-bit resolution).
Remark The result of A/D conversion by this API function must be read within the maximum pending time of the ΔΣ A/D conversion result register n after ΔΣ A/D conversion end interrupt INTDSAD is generated.
[Syntax]
#include “r_cg_macrodriver.h”
void R_DSADC_Channeln_Get_Result_16bit ( uint16_t * const buffer );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       Uint16_t * const buffer;  | 
    
       Pointer to area in which to store the results of A/D conversion  | 
[Return value]
None.