Reads the data from Data Flash Memories.
[Syntax]
pfdl_status_t R_FDL_Read ( pfdl_u16 index, __near pfdl_u08 * buffer, pfdl_u16 bytecount );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
pfdl_u16 index; |
Reading start address of the Data Flash Memories |
|
I |
pfdl_u08 * buffer; |
Pointer to a buffer to store the read data |
|
I |
pfdl_u16 bytecount; |
Total amount of data to read |
[Return value]
|
マクロ |
Description |
|
PFDL_OK |
Normal completion |
|
PFDL_BUSY |
During execution of the other commands. |
|
PFDL_ERR_PARAMETER |
Error of the parameters |