Starts IICA slave reception.
Remark This API function performs byte-level IICA slave reception the number of times specified by the argument rx_num, and stores the data in the buffer specified by the argument rx_buf.
[Syntax]
#include “r_cg_macrodriver.h”
void R_IICAn_Slave_Receive ( uint8_t * const rx_buf, uint16_t rx_num );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint8_t * const rx_buf;  | 
    
       Pointer to a buffer to store the received data  | 
| 
       I  | 
    
       uint16_t rx_num;  | 
    
       Total amount of data to receive  | 
[Return value]
None.