Usage example
Get the A/D conversion result of 2 pins.
[GUI setting example]
| 12-Bit A/D convertor | ||||
| ADC | Used | |||
| A/D convertor operation setting | Used | |||
| A/D conversion clock setting | PCLK | |||
| A/D conversion mode setting | High-speed conversion | |||
| VREF(+)setting | AVDD | |||
| VREF(-)setting | AVSS | |||
| Operation mode setting | Single scan mode | |||
| 
 | 
 | 
 | Conversion start trigger setting | Software trigger | 
| 
 | 
 | 
 | Analog input channel setting | 
 | 
| 
 | 
 | 
 | ANI00 | Used | 
| 
 | 
 | 
 | ANI00 addition/Average function | Unused | 
| 
 | 
 | 
 | ANI01 | Used | 
| 
 | 
 | 
 | ANI01 addition/Average function | Unused | 
| 
 | 
 | 
 | Data registers setting | 
 | 
| 
 | 
 | 
 | ADconversion value addition count | 1-time conversion | 
| 
 | 
 | 
 | Data placement | Right-alignment | 
| 
 | 
 | 
 | Automatic clearing | Disable automatic clearing | 
| 
 | 
 | 
 | ANI00 input sampling time | 3.667(μs) (Actual value:3.667) | 
| 
 | 
 | 
 | ANI01 input sampling time | 3.667(μs) (Actual value:3.667) | 
| 
 | 
 | 
 | A/D converted value count setting | Addition mode | 
| 
 | 
 | 
 | Interrupt setting | Enable AD conversion end interrupt(INTAD) | 
| 
 | 
 | 
 | Priority | Level 3 (Low Priority) | 
[API setting example]
r_cg_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start AD converter */
R_12ADC_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_12adc_user.c
/* Start user code for global. Do not edit comment generated here */
volatile uint16_t g_12adc_ch000_value;
volatile uint16_t g_12adc_ch001_value;
/* End user code. Do not edit comment generated here */
static void __near r_12adc_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Stop AD converter */
R_12ADC_Stop();
/* Get AD converter result */
R_12ADC_Get_ValueResult(ADCHANNEL0, (uint16_t *)&g_12adc_ch000_value);
R_12ADC_Get_ValueResult(ADCHANNEL1, (uint16_t *)&g_12adc_ch001_value);
/* End user code. Do not edit comment generated here */
}