Usage example (Timer mode)
Enter the interrupt function at fixed intervals and count the number of interrupt occurrence.
[Waveform example]

[GUI setting example]
| 
       Timer  | 
    
       Used  | |||
| 
       TMRJ0  | 
    
       Used  | |||
| 
       Functions  | 
    
       Timer mode  | |||
| 
       Count source setting  | 
    
       Auto  | |||
| 
       Timer value  | 
    
       100μs (Actual value:100)  | |||
| 
       When the counter underflows, generate an interrupt (INTTRJ0)  | 
    
       Used  | |||
| 
       Priority  | 
    
       Low  | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start TMRJ0 counter */
R_TMR_RJ0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}
r_cg_timer_user.c
/* Start user code for global. Do not edit comment generated here */
volatile uint8_t g_cnt = 0U;
/* End user code. Do not edit comment generated here */
static void __near r_tmr_rj0_interrupt(void)
{
/* Start user code. Do not edit comment generated here */
/* Count INTTRJ0 */
g_cnt++;
/* End user code. Do not edit comment generated here */
}