Everything

R_DOC_WriteData

Sets the value for comparison with, addition to, or subtraction from the reference value.

 

[Syntax]

void    R_DOC_WriteData ( uint16_t data );

 

[Argument(s)]

I/O

Argument

Description

I

uint16_t data;

Input data for use in operation

 

[Return value]

None.